Skip to main content

Crystal Tower

Bucharest, Romania

Dazzling energy-efficient landmark

The Crystal Tower in central Bucharest is home to the Romanian headquarters of ING Bank. The stunning office building was designed by architect Adrian Spirescu to look like a crystal uncovered in the grey stone that is predominant in the Romanian capital. This affect is achieved by the building’s asymmetric profile, with a glass façade cut at different angles. Unique to Bucharest, the tower is also topped with a helipad.

bg-image

The tower’s striking and innovative design is matched by a number of innovative and sustainable features, including a double-skin glass façade. This design is just one of the features we used to help Crystal Tower achieve more energy efficiency and a BREEAM "Excellent" rating.

The building developers wanted a modern, energy-efficient and versatile air conditioning solution for the entire building.

"Ultimately, we wanted an energy-efficient building and Daikin provided the optimum solution."

- SC Plaza Development srl

A major achievement in sustainable building and design

To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution. As one of the few manufacturers to offer this kind of solution, we were able to help this high-rise building achieve heating, cooling, ventilation and hot water and optimise each for large and small spaces.

Crystal Tower won the Bucharest Architecture "Eco Architecture Award" in 2012 and was also named as "Green Project of the Year" by the Romanian Green Building Council. It is a shining example of how an innovative building design, combined with the latest climate control technology, can deliver highly sustainable results for tall buildings in urban environments.

Solution at a glance

This installation included a surface area of 16,900m2 (15 floors in total). In addition to a water loop for VRV water-cooled modules, boilers and cooling towers, this installation also includes:

  • 3 VRV III outdoor units 
  • 67 water-cooled VRV outdoor units 
  • 265 concealed ceiling units 
  • 24 4-way blow cassette units 
  • 5 Sky Air outdoor units 
  • 5 4-way blow cassette units 
  • 1 air-cooled multi-scroll chiller 
  • 1 air-cooled screw chiller 
  • 11 BACnet interface

Learn more

Our other cases

  • ACTION

    As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
  • Action reclaimed refrigerant allocation

    Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
  • CA

    Looking to renovate its entire HVAC system, the CA store wanted to achieve year-round comfort in the most cost-effective and efficient way.
  • City Centre Hotel

    Chiller change boosts comfort at central London hotel.
  • Coral betting office

    Discover how our auto-cleaning roundflow cassettes achieved 50 more energy savings for Coral betting offices.
  • Courtyard Hotel Paris

    The Courtyard conversion marks a successful collaboration between forward- looking urban regeneration and Daikin’s flexible, future-proof VRV heat recovery technology.
  • Crédit Agricole

    Known as "the green bank" due to its agricultural history, Crédit Agricole wanted an energy efficient and low maintenance air conditioning solution for one of its branches.
  • Crystal Tower

    To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.
  • Holcim cement plant

    The Holcim cement plant relies on state-of-the-art technology to achieve its ambitious environmental and energy-efficiency goals.
  • JBC

    In its ongoing search to optimise running costs, JBC conducted a site trial with Daikin designed to evaluate the gains generated by Variable Refrigerant Temperature VRT technology.
  • K-Way

    When high-end clothing retailer K-Way opened a new store in Covet Garden, London, we worked with nation-wide D1 contractor Royale to devise and install the perfect energy-efficient solution for the property.
  • Leon's restaurant

    M&E contractor, Synecore, installed its first ‘invisible’ HVAC system, the Daikin VRV IV i-Series at Leon Restaurant, central London, to overcome tight space restrictions and achieve maximum climate control efficiency.
  • Naturkost Brinkman

    Organic specialist retailer Naturkost Brinkman uses Daikin retail refrigeration to deliver improved energy efficiency and in-store comfort.
  • Pomme d'Or Hotel

    Air conditioning has become the norm in most new and refurbished hotels. Today’s systems keep guests cool during summer – and additionally provide cost-efficient heating during winter periods. Daikin heat pumps use renewable energy to do this, cutting hotel operating costs. And there’s also a positive impact on indoor aesthetics.
  • Hotel Santos Porta Fira

    The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
  • The Post Hotel

    As climate control specialists, we chose our VRV system for the Post Hotel Ghent for its combination of energy-efficient technology and ability to provide more comfort.
  • Samrya 44

    With 44 floors of elegantly-designed luxury suites, Samrya 44 adheres only to the highest standards in construction and HVAC.
  • Sportisimo

    For this project, we chose to install an outdoor system that connects to a variety of indoor and ventilation units strategically placed in the shop.
  • The Bloomsbury Hotel

    The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
  • Torre Serenissima

    Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
  • Van der Valk Hotel

    From the lobby to the guest rooms to the kitchen, every space in the Van der Valk Hotel has its own unique climate needs. Our goal was to develop an integrated system to meet the needs of each of these locations and lower the total environmental impact of the system.
  • Velocity office building

    Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
  • Venetian Arsenal

    An innovative climate control system that taps into the natural energy of the Venetian Lagoon is delivering high levels of comfort and energy efficiencies while preserving an historic industrial building in the heart of Venice.
  • VMD business centre

    A VRV IV system is providing all the heating and cooling for VMD Tower B, a 25-storey office building in Zagreb, helping it to meet the highest levels of efficiency and lowering energy consumption.

Find more information

Take a tour in our virtual showroom

Need help?

Read our news

Read our blog

Get inspired from references

Find more information

Need help?

Need help?