Skip to main content

The Bloomsbury Hotel

London, UK

bg-image

Designed in the 1930s by renowned British Architect, Sir Edwin Lutyens, The Bloomsbury Hotel already underwent a sensitive restoration to become the chic heritage hotel it is today. Retaining many of its original architectural features, the iconic hotel hosts a double-height lobby, elegant prohibition era bar, library and 153 guests rooms and suites. The hotel also hosts a variety of meetings rooms and event halls of all sizes, as well as fully equipped dining areas and kitchens.

Seeking comfort with improved environmental standards

The Doyle Collection, the owners of the hotel, wanted to lower the building's energy usage and cut CO2 emissions by 30%. They also sought to improve comfort levels for guests by optimising climate control in all guest rooms, meeting spaces, and in the bar and restaurant. Keeping to a nine-month programme was essential to ensure minimal revenue losses.

"The challenge for this project was to preserve the historic interior and exterior of the building. With Daikin VRV, we knew that we could easily take on this challenge and improve our system's energy efficiency. Along with Daikin UK, this was a great team effort—showing the benefit of a strong and lasting working relationship between client and contractor."

- Michael Neve, General Manager, The Bloomsbury Hotel

Fully efficient system replacement with minimal disruption

For this project, we installed 56 outdoor units linked to 209 indoor ducted and wall-mounted concealed units in the guest rooms. For the communal areas we chose to install a mixture of wall-mounted and floor standing units.

Our VRV-Q system was the perfect choice for The Bloomsbury Hotel because the units are energy-efficient and flexible. Equipped with refrigerant R-410A but functioning at a pressure level like most refrigerant R-22 systems, VRV-Q units are 40% more efficient in heating and 25% more in cooling than an R-22 system.

Compact and lightweight, VRV-Q units are easy to install and cost-effective because they use existing piping and wiring. This means the renovation price was cut in half because it does not need a full pipe replacement. Installing the VRV-Q units floor-by-floor also allowed the hotel to stay open during the renovation.

bg-image

Solution at a glance

bg-image
  • 209 indoor units (concealed ceiling + wall-mounted units)
  • 56 VRV III-Q replacement outdoor units (heat recovery)
  • Intelligent Touch Manager

Learn more

Our other cases

  • ACTION

    As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
  • Action reclaimed refrigerant allocation

    Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
  • CA

    Looking to renovate its entire HVAC system, the CA store wanted to achieve year-round comfort in the most cost-effective and efficient way.
  • City Centre Hotel

    Chiller change boosts comfort at central London hotel.
  • Coral betting office

    Discover how our auto-cleaning roundflow cassettes achieved 50 more energy savings for Coral betting offices.
  • Courtyard Hotel Paris

    The Courtyard conversion marks a successful collaboration between forward- looking urban regeneration and Daikin’s flexible, future-proof VRV heat recovery technology.
  • Crédit Agricole

    Known as "the green bank" due to its agricultural history, Crédit Agricole wanted an energy efficient and low maintenance air conditioning solution for one of its branches.
  • Crystal Tower

    To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.
  • Holcim cement plant

    The Holcim cement plant relies on state-of-the-art technology to achieve its ambitious environmental and energy-efficiency goals.
  • JBC

    In its ongoing search to optimise running costs, JBC conducted a site trial with Daikin designed to evaluate the gains generated by Variable Refrigerant Temperature VRT technology.
  • K-Way

    When high-end clothing retailer K-Way opened a new store in Covet Garden, London, we worked with nation-wide D1 contractor Royale to devise and install the perfect energy-efficient solution for the property.
  • Leon's restaurant

    M&E contractor, Synecore, installed its first ‘invisible’ HVAC system, the Daikin VRV IV i-Series at Leon Restaurant, central London, to overcome tight space restrictions and achieve maximum climate control efficiency.
  • Naturkost Brinkman

    Organic specialist retailer Naturkost Brinkman uses Daikin retail refrigeration to deliver improved energy efficiency and in-store comfort.
  • Pomme d'Or Hotel

    Air conditioning has become the norm in most new and refurbished hotels. Today’s systems keep guests cool during summer – and additionally provide cost-efficient heating during winter periods. Daikin heat pumps use renewable energy to do this, cutting hotel operating costs. And there’s also a positive impact on indoor aesthetics.
  • Hotel Santos Porta Fira

    The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
  • The Post Hotel

    As climate control specialists, we chose our VRV system for the Post Hotel Ghent for its combination of energy-efficient technology and ability to provide more comfort.
  • Samrya 44

    With 44 floors of elegantly-designed luxury suites, Samrya 44 adheres only to the highest standards in construction and HVAC.
  • Sportisimo

    For this project, we chose to install an outdoor system that connects to a variety of indoor and ventilation units strategically placed in the shop.
  • The Bloomsbury Hotel

    The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
  • Torre Serenissima

    Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
  • Van der Valk Hotel

    From the lobby to the guest rooms to the kitchen, every space in the Van der Valk Hotel has its own unique climate needs. Our goal was to develop an integrated system to meet the needs of each of these locations and lower the total environmental impact of the system.
  • Velocity office building

    Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
  • Venetian Arsenal

    An innovative climate control system that taps into the natural energy of the Venetian Lagoon is delivering high levels of comfort and energy efficiencies while preserving an historic industrial building in the heart of Venice.
  • VMD business centre

    A VRV IV system is providing all the heating and cooling for VMD Tower B, a 25-storey office building in Zagreb, helping it to meet the highest levels of efficiency and lowering energy consumption.

Find more information

Take a tour in our virtual showroom

Need help?

Read our news

Read our blog

Get inspired from references

Find more information

Need help?

Need help?