Skip to main content

JBC

Vilvoorde, Belgium

bg-image

Swept up in the relentless pace of life in the 21st century, today’s shoppers really appreciate the chance to relax, kick back and enjoy a little retail therapy. This quest for wellbeing – and the fact that shoppers who feel comfortable shop for longer and spend more – is something that the ready-to-wear fashion chain JBC has long been aware of. In fact, over the past years, JBC has worked closely with Daikin to provide just the right level of climate control and comfort in all of its stores.

More recently, in its ongoing search to optimise running costs still further, JBC conducted a site trial with Daikin designed to evaluate the potential gains generated by Variable Refrigerant Temperature (VRT) technology. The results of the test were more than conclusive.

“Having a comfortable climate in the shop is crucial for customer satisfaction and retention.”

- Gert Laeveren, JBC

VRT technology put to the test

To obtain an accurate comparison of the running costs and comfort levels of the VRT technology, two identical Sky Air outdoor units were used, each connected to Daikin’s unique Round Flow Cassette system. 

One system for the test featured Daikin’s VRT technology, which balances the refrigerant temperature to match the actual load in the room, while the other system did not have the VRT function enabled. To ensure identical operating times and settings to provide an accurate comparison, the two units were connected to the same remote control unit, with the same room temperature, fan speed, airflow rate, etc.

Both Sky Air outdoor units were also connected to a kWh meter to measure their actual power consumption precisely. This data was collected for every minute of the day, from June 2017 to May 2018. The ongoing readings were monitored and reported remotely using the Daikin Cloud Service.

VRV IV

Lower costs, greater comfort

The VRT-enabled unit performed considerably better in terms of energy consumption and comfort, for both visitors to the store and shop staff alike.

From an energy efficiency point of view, the VRT system consumed up to 21% less power in mild conditions, with annual savings recorded at an Impressive 14%. Multiply that figure over the total number of JBC stores and you have an idea of just how much JBC can save on its running costs by using VRT technology – quite apart from keeping customers comfortable while they spend money, and also the benefit for the environment.

Learn more

Our other cases

  • ACTION

    As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
  • Action reclaimed refrigerant allocation

    Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
  • CA

    Looking to renovate its entire HVAC system, the CA store wanted to achieve year-round comfort in the most cost-effective and efficient way.
  • City Centre Hotel

    Chiller change boosts comfort at central London hotel.
  • Coral betting office

    Discover how our auto-cleaning roundflow cassettes achieved 50 more energy savings for Coral betting offices.
  • Courtyard Hotel Paris

    The Courtyard conversion marks a successful collaboration between forward- looking urban regeneration and Daikin’s flexible, future-proof VRV heat recovery technology.
  • Crédit Agricole

    Known as "the green bank" due to its agricultural history, Crédit Agricole wanted an energy efficient and low maintenance air conditioning solution for one of its branches.
  • Crystal Tower

    To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.
  • Holcim cement plant

    The Holcim cement plant relies on state-of-the-art technology to achieve its ambitious environmental and energy-efficiency goals.
  • JBC

    In its ongoing search to optimise running costs, JBC conducted a site trial with Daikin designed to evaluate the gains generated by Variable Refrigerant Temperature VRT technology.
  • K-Way

    When high-end clothing retailer K-Way opened a new store in Covet Garden, London, we worked with nation-wide D1 contractor Royale to devise and install the perfect energy-efficient solution for the property.
  • Leon's restaurant

    M&E contractor, Synecore, installed its first ‘invisible’ HVAC system, the Daikin VRV IV i-Series at Leon Restaurant, central London, to overcome tight space restrictions and achieve maximum climate control efficiency.
  • Naturkost Brinkman

    Organic specialist retailer Naturkost Brinkman uses Daikin retail refrigeration to deliver improved energy efficiency and in-store comfort.
  • Pomme d'Or Hotel

    Air conditioning has become the norm in most new and refurbished hotels. Today’s systems keep guests cool during summer – and additionally provide cost-efficient heating during winter periods. Daikin heat pumps use renewable energy to do this, cutting hotel operating costs. And there’s also a positive impact on indoor aesthetics.
  • Hotel Santos Porta Fira

    The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
  • The Post Hotel

    As climate control specialists, we chose our VRV system for the Post Hotel Ghent for its combination of energy-efficient technology and ability to provide more comfort.
  • Samrya 44

    With 44 floors of elegantly-designed luxury suites, Samrya 44 adheres only to the highest standards in construction and HVAC.
  • Sportisimo

    For this project, we chose to install an outdoor system that connects to a variety of indoor and ventilation units strategically placed in the shop.
  • The Bloomsbury Hotel

    The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
  • Torre Serenissima

    Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
  • Van der Valk Hotel

    From the lobby to the guest rooms to the kitchen, every space in the Van der Valk Hotel has its own unique climate needs. Our goal was to develop an integrated system to meet the needs of each of these locations and lower the total environmental impact of the system.
  • Velocity office building

    Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
  • Venetian Arsenal

    An innovative climate control system that taps into the natural energy of the Venetian Lagoon is delivering high levels of comfort and energy efficiencies while preserving an historic industrial building in the heart of Venice.
  • VMD business centre

    A VRV IV system is providing all the heating and cooling for VMD Tower B, a 25-storey office building in Zagreb, helping it to meet the highest levels of efficiency and lowering energy consumption.

Find more information

Take a tour in our virtual showroom

Need help?

Read our news

Read our blog

Get inspired from references

Find more information

Need help?

Need help?