Skip to main content

Naturkost Brinkman

Warburg, Germany

bg-image

Naturkost Brinkman is a successful organic specialist retailer. In 2017, the company embarked on a store expansion programme to create additional retail space and to accommodate new customer and staff facilities.

A primary focus for the company was the adoption of new future-proof, reliable and innovating technologies to increase energy efficiency and to provide an enhanced shopping experience for customers. 

"The Daikin concept was a perfect fit with our desire to use the waste heat from the refrigeration cabinets. We considered other solutions, but Daikin's concept was ultimately the most economical"

- Gerrit Brinkman, Naturkost Brinkman

All round solution

Naturkost Brinkman opted for Daikin's plug-in Conveni-Pack combined system. Designed specifically to meet the requirements of food retailers, Conveni-Pack offers a total solution which integrates refrigeration, freezing, air conditioning and ventilation in one compact unit, making it an ideal replacement solution.

Integral heat recovery technology enables the redistribution of waste heat from the refrigeration units to the store’s retail areas. Plug and play functionality assures fast installation, with high operational reliability offering low maintenance costs for the customer.

A Daikin VRV IV air-to-air heat pump system provides additional heating to the store, offices, social areas and toilets. A total of eight indoor units are connected to the VRV system.

bg-image

Low noise systems

Sound absorbers in the machinery room ventilation system

Due to the location of the store in the densely populated city centre of Warburg, there were stringent requirements in terms of noise protection. “We installed all the refrigeration equipment inside the building, in the newly created machinery room. Sound absorbers were also integrated into the machinery room ventilation system,” explains Franko Bitaris of Friedrich Hertel Kälte & Klimatechnik GmbH & Co.KG.

Environmentally-friendly building technology

With the new refrigeration and air-conditioning technology in place, Naturkost Brinkman is well positioned for the future. The intelligent use of renewable heat pump technology and waste heat recovery makes it possible to use energy in a resource-saving way, focusing on the environmental aspect while saving on energy costs.

The Daikin intelligent Touch Manager controller ensures efficient operation and further reduces energy consumption.

Naturkost Brinkman Daikin intelligent Touch Manager

Learn more

Our other cases

  • ACTION

    As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
  • Action reclaimed refrigerant allocation

    Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
  • CA

    Looking to renovate its entire HVAC system, the CA store wanted to achieve year-round comfort in the most cost-effective and efficient way.
  • City Centre Hotel

    Chiller change boosts comfort at central London hotel.
  • Coral betting office

    Discover how our auto-cleaning roundflow cassettes achieved 50 more energy savings for Coral betting offices.
  • Courtyard Hotel Paris

    The Courtyard conversion marks a successful collaboration between forward- looking urban regeneration and Daikin’s flexible, future-proof VRV heat recovery technology.
  • Crédit Agricole

    Known as "the green bank" due to its agricultural history, Crédit Agricole wanted an energy efficient and low maintenance air conditioning solution for one of its branches.
  • Crystal Tower

    To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.
  • Holcim cement plant

    The Holcim cement plant relies on state-of-the-art technology to achieve its ambitious environmental and energy-efficiency goals.
  • JBC

    In its ongoing search to optimise running costs, JBC conducted a site trial with Daikin designed to evaluate the gains generated by Variable Refrigerant Temperature VRT technology.
  • K-Way

    When high-end clothing retailer K-Way opened a new store in Covet Garden, London, we worked with nation-wide D1 contractor Royale to devise and install the perfect energy-efficient solution for the property.
  • Leon's restaurant

    M&E contractor, Synecore, installed its first ‘invisible’ HVAC system, the Daikin VRV IV i-Series at Leon Restaurant, central London, to overcome tight space restrictions and achieve maximum climate control efficiency.
  • Naturkost Brinkman

    Organic specialist retailer Naturkost Brinkman uses Daikin retail refrigeration to deliver improved energy efficiency and in-store comfort.
  • Pomme d'Or Hotel

    Air conditioning has become the norm in most new and refurbished hotels. Today’s systems keep guests cool during summer – and additionally provide cost-efficient heating during winter periods. Daikin heat pumps use renewable energy to do this, cutting hotel operating costs. And there’s also a positive impact on indoor aesthetics.
  • Hotel Santos Porta Fira

    The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
  • The Post Hotel

    As climate control specialists, we chose our VRV system for the Post Hotel Ghent for its combination of energy-efficient technology and ability to provide more comfort.
  • Samrya 44

    With 44 floors of elegantly-designed luxury suites, Samrya 44 adheres only to the highest standards in construction and HVAC.
  • Sportisimo

    For this project, we chose to install an outdoor system that connects to a variety of indoor and ventilation units strategically placed in the shop.
  • The Bloomsbury Hotel

    The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
  • Torre Serenissima

    Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
  • Van der Valk Hotel

    From the lobby to the guest rooms to the kitchen, every space in the Van der Valk Hotel has its own unique climate needs. Our goal was to develop an integrated system to meet the needs of each of these locations and lower the total environmental impact of the system.
  • Velocity office building

    Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
  • Venetian Arsenal

    An innovative climate control system that taps into the natural energy of the Venetian Lagoon is delivering high levels of comfort and energy efficiencies while preserving an historic industrial building in the heart of Venice.
  • VMD business centre

    A VRV IV system is providing all the heating and cooling for VMD Tower B, a 25-storey office building in Zagreb, helping it to meet the highest levels of efficiency and lowering energy consumption.

Find more information

Take a tour in our virtual showroom

Need help?

Read our news

Read our blog

Get inspired from references

Find more information

Need help?

Need help?