Skip to main content

Holcim cement plant

Dotternhausen, Germany

bg-image

Minimizing the impact on the environment and the local population is a top priority at the Holcim cement plant in Dotternhausen, Germany. Cement production consumes a great deal of energy due to the high temperatures required. That’s why the Holcim cement plant relies on state-of-the-art technology to achieve its ambitious environmental and energy-efficiency goals.

A chiller from Daikin featuring leading-edge technologies designed ensure high energy efficiency and low energy costs is helping the company meet these goals.

"The chiller is helping us achieve the environmental and energy-efficiency goals of Holcim Süddeutschland GmbH) at the Dotternhausen cement plant. These Include reducing harmful emissions, especially CO2 emissions, conserving natural resources and increasing energy efficiency."

- Stephen Mocker, Holcim (Süddeutschland) GmbH

Challenging requirements for cooling and reliability, as well as installation

Holcim has relied on Daikin technology in its server and transformer rooms for many years. In 2016, the company also began using a chiller from Daikin to neutralize the heat that the cement mill generates during grinding operations on drives, bearings and on the hydraulic circuit as well as to cool the compressors in the central compressed-air station. These applications place high demands on chiller performance, since the material is previously heated to 1400 °C in the rotary kiln.

The installation of the chiller took place under difficult conditions, with the technicians having only three hours to integrate it. In the event of a prolonged stoppage, the air compressors become overheated and switch off – shutting down operations, since the plant’s systems cannot run without compressed air. Daikin’s plug-and-play solutions enabled these challenging demands to be met, with systems supplied ready for installation and operation.

Installation

Reducing the cement plant’s CO2 emissions

bg-image

As a binder for concrete, cement is an integral part of our lives, which is found in everything from roads to factory, office and residential buildings. Holcim focuses on making cement and binder from fired oil shale – a production process that cuts CO2 emissions. Clinker production consumes a great deal of energy due to the high temperatures needed to burn the limestone, making it difficult to optimise the production process in terms of energy consumption.

Holcim nevertheless wants to live up to its environmental responsibility by giving top priority to the use of energy-efficient systems. The company is upgrading its existing systems in a targeted manner, while focusing on enhancing efficiency for new investments.

Daikin chillers offer outstanding operation while also minimising energy consumption.

Learn more

Our other cases

  • ACTION

    As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
  • Action reclaimed refrigerant allocation

    Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
  • CA

    Looking to renovate its entire HVAC system, the CA store wanted to achieve year-round comfort in the most cost-effective and efficient way.
  • City Centre Hotel

    Chiller change boosts comfort at central London hotel.
  • Coral betting office

    Discover how our auto-cleaning roundflow cassettes achieved 50 more energy savings for Coral betting offices.
  • Courtyard Hotel Paris

    The Courtyard conversion marks a successful collaboration between forward- looking urban regeneration and Daikin’s flexible, future-proof VRV heat recovery technology.
  • Crédit Agricole

    Known as "the green bank" due to its agricultural history, Crédit Agricole wanted an energy efficient and low maintenance air conditioning solution for one of its branches.
  • Crystal Tower

    To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.
  • Holcim cement plant

    The Holcim cement plant relies on state-of-the-art technology to achieve its ambitious environmental and energy-efficiency goals.
  • JBC

    In its ongoing search to optimise running costs, JBC conducted a site trial with Daikin designed to evaluate the gains generated by Variable Refrigerant Temperature VRT technology.
  • K-Way

    When high-end clothing retailer K-Way opened a new store in Covet Garden, London, we worked with nation-wide D1 contractor Royale to devise and install the perfect energy-efficient solution for the property.
  • Leon's restaurant

    M&E contractor, Synecore, installed its first ‘invisible’ HVAC system, the Daikin VRV IV i-Series at Leon Restaurant, central London, to overcome tight space restrictions and achieve maximum climate control efficiency.
  • Naturkost Brinkman

    Organic specialist retailer Naturkost Brinkman uses Daikin retail refrigeration to deliver improved energy efficiency and in-store comfort.
  • Pomme d'Or Hotel

    Air conditioning has become the norm in most new and refurbished hotels. Today’s systems keep guests cool during summer – and additionally provide cost-efficient heating during winter periods. Daikin heat pumps use renewable energy to do this, cutting hotel operating costs. And there’s also a positive impact on indoor aesthetics.
  • Hotel Santos Porta Fira

    The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
  • The Post Hotel

    As climate control specialists, we chose our VRV system for the Post Hotel Ghent for its combination of energy-efficient technology and ability to provide more comfort.
  • Samrya 44

    With 44 floors of elegantly-designed luxury suites, Samrya 44 adheres only to the highest standards in construction and HVAC.
  • Sportisimo

    For this project, we chose to install an outdoor system that connects to a variety of indoor and ventilation units strategically placed in the shop.
  • The Bloomsbury Hotel

    The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
  • Torre Serenissima

    Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
  • Van der Valk Hotel

    From the lobby to the guest rooms to the kitchen, every space in the Van der Valk Hotel has its own unique climate needs. Our goal was to develop an integrated system to meet the needs of each of these locations and lower the total environmental impact of the system.
  • Velocity office building

    Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
  • Venetian Arsenal

    An innovative climate control system that taps into the natural energy of the Venetian Lagoon is delivering high levels of comfort and energy efficiencies while preserving an historic industrial building in the heart of Venice.
  • VMD business centre

    A VRV IV system is providing all the heating and cooling for VMD Tower B, a 25-storey office building in Zagreb, helping it to meet the highest levels of efficiency and lowering energy consumption.

Find more information

Take a tour in our virtual showroom

Need help?

Read our news

Read our blog

Get inspired from references

Find more information

Need help?

Need help?