Skip to main content

Venetian Arsenal

Venice, Italy

bg-image

Once the centre of Venice's naval power, the Venetian Arsenale was once a maritime base composed of Byzantine-style buildings covering about 15% of the city. To preserve these historic buildings, the Ministry of Infrastructure and Transport - Venice Water Authority, turned them into brand new offices, homes and cultural institutions. Our goal was to deliver the right climate control solution to provide heating and hot water for the buildings, without disrupting the existing architecture and infrastructure.

Resourceful and sustainable climate control

We decided to take advantage of the abundant natural resource on the city's doorstep: water. To do this, we installed a water-cooled VRV system to extract thermal energy to provide heating and hot water for the Venice Arsenale complex.

Each building uses a heat pump attached to a water-loop system which connects several buildings in one complex. By installing the same system in each building, excess heat can easily transfer from one building to another in need of heating or hot water.

Through this process, our water-cooled VRV system easily achieved higher energy efficiency. It also served as the perfect solution for a sensitive restoration project such as the Venetian Arsenale because it is discreet and avoided disrupting existing architecture.

Venitian arsenal architecture

The Generatori building

bg-image

One of the more recent buildings benefiting from the Venetian Arsenale renovation project was the Generatori building. A 3-storey building dating back to 1900, the Generatori building initially supplied electricity to the shipyards, and now serves as a space for offices, meeting rooms and archives.

The building uses a water-cooled VRV system to supply underfloor heating for the ground floor reception hall, meeting rooms and basement, as well as fan coil units to provide cooling and heating on the two upper floors of office space. There are also ventilation units throughout the building to ensure the air is fresh and pure. A control system enables occupants to individually control the temperature of different zones while linking it all back to a central management system.

Our VRV system was the ideal choice for this project as it could easily be connected to the water-loop to achieve a stable and comfortable climate with higher energy efficiency.

Solution at a glance

  • 1 BACnet interface to connect to the BMS system
  • 1 Intelligent Touch controller for central control
  • 1 heat reclaim ventilation unit (VAM)
  • 2 hot water hydroboxes to provide hot water
  • 20 medium and 2 high static pressure concealed ceiling indoor units
  • 2 concealed floor standing units
  • 8 water-cooled VRV outdoor units with BS boxes allowing heat recovery
bg-image

Learn more

Our other cases

  • ACTION

    As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
  • Action reclaimed refrigerant allocation

    Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
  • CA

    Looking to renovate its entire HVAC system, the CA store wanted to achieve year-round comfort in the most cost-effective and efficient way.
  • City Centre Hotel

    Chiller change boosts comfort at central London hotel.
  • Coral betting office

    Discover how our auto-cleaning roundflow cassettes achieved 50 more energy savings for Coral betting offices.
  • Courtyard Hotel Paris

    The Courtyard conversion marks a successful collaboration between forward- looking urban regeneration and Daikin’s flexible, future-proof VRV heat recovery technology.
  • Crédit Agricole

    Known as "the green bank" due to its agricultural history, Crédit Agricole wanted an energy efficient and low maintenance air conditioning solution for one of its branches.
  • Crystal Tower

    To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.
  • Holcim cement plant

    The Holcim cement plant relies on state-of-the-art technology to achieve its ambitious environmental and energy-efficiency goals.
  • JBC

    In its ongoing search to optimise running costs, JBC conducted a site trial with Daikin designed to evaluate the gains generated by Variable Refrigerant Temperature VRT technology.
  • K-Way

    When high-end clothing retailer K-Way opened a new store in Covet Garden, London, we worked with nation-wide D1 contractor Royale to devise and install the perfect energy-efficient solution for the property.
  • Leon's restaurant

    M&E contractor, Synecore, installed its first ‘invisible’ HVAC system, the Daikin VRV IV i-Series at Leon Restaurant, central London, to overcome tight space restrictions and achieve maximum climate control efficiency.
  • Naturkost Brinkman

    Organic specialist retailer Naturkost Brinkman uses Daikin retail refrigeration to deliver improved energy efficiency and in-store comfort.
  • Pomme d'Or Hotel

    Air conditioning has become the norm in most new and refurbished hotels. Today’s systems keep guests cool during summer – and additionally provide cost-efficient heating during winter periods. Daikin heat pumps use renewable energy to do this, cutting hotel operating costs. And there’s also a positive impact on indoor aesthetics.
  • Hotel Santos Porta Fira

    The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
  • The Post Hotel

    As climate control specialists, we chose our VRV system for the Post Hotel Ghent for its combination of energy-efficient technology and ability to provide more comfort.
  • Samrya 44

    With 44 floors of elegantly-designed luxury suites, Samrya 44 adheres only to the highest standards in construction and HVAC.
  • Sportisimo

    For this project, we chose to install an outdoor system that connects to a variety of indoor and ventilation units strategically placed in the shop.
  • The Bloomsbury Hotel

    The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
  • Torre Serenissima

    Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
  • Van der Valk Hotel

    From the lobby to the guest rooms to the kitchen, every space in the Van der Valk Hotel has its own unique climate needs. Our goal was to develop an integrated system to meet the needs of each of these locations and lower the total environmental impact of the system.
  • Velocity office building

    Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
  • Venetian Arsenal

    An innovative climate control system that taps into the natural energy of the Venetian Lagoon is delivering high levels of comfort and energy efficiencies while preserving an historic industrial building in the heart of Venice.
  • VMD business centre

    A VRV IV system is providing all the heating and cooling for VMD Tower B, a 25-storey office building in Zagreb, helping it to meet the highest levels of efficiency and lowering energy consumption.

Find more information

Take a tour in our virtual showroom

Need help?

Read our news

Read our blog

Get inspired from references

Find more information

Need help?

Need help?